2/9/2022 8:11 PM | |
Joined: 7/2/2015 Last visit: 8/25/2025 Posts: 96 Rating:
|
Hi nesrine.tn, You can check the example "Redundancy in WinCC V7.x and WinCC Professional". There you can find the chapter "2.3 Requirements for Redundant Systems" that can clarify you a little bit. Furthermore is recommended to have a CP or IE card for the following elements: 1st CP/ IE card for redundancy bus (only each server WinCC PC is connected to that network) 2nd CP/ IE card for terminal bus (every client must connect on this network) 3rd CP/IE card for fiel bus (on this network you connect PLCs, Periphery, Drives... every field element) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on