2/10/2022 1:55 PM | |
Joined: 4/15/2015 Last visit: 6/14/2022 Posts: 12 Rating:
|
Available: CPU 224XP 6ES7214-2BD23-0XB0. LINK: https://support.industry.siemens.com/cs/pd/222942?pdti=pi&dl=en&lc=en-ww SIMATIC HMI KTP700 BASIC DP 6AV2123-2GA03-0AX0 LINK: https://support.industry.siemens.com/cs/pd/233386?pdti=pi&dl=en&lc=en-us Adapter for communication with CPU: 6ES7901-3DB30-0XA0 Adapter for communication with Panel HMI: 6GK1571-0BA00-0AA0 data exchange cable <---------> PLC Standard shielded Profibus PROFIBUS cable (6xv1830-0EH10) Connector to the RS 485 6ES7 972-0BB42-0XA0 bus He studied: https://cache.industry.siemens.com/dl/files/582/1109582/att_22063/v1/s7200_system_manual_en-ust.pdf. Communicating Over A Network Chapter 7 Page 211-217 Communication with CPU set up (see photo connection). Access CPU on both ports (Port 0 & Port 1). [see System Block] /////////////////////// /\\\\\\\\\\\\\\\\\\\\\\\\\\\ \\\\ Setting up the SIMATIC HMI KTP700 Basic DP panel in Tia Portal V14 SP1 Connection: (See photo Connections) PPI protocol BAUD RATE: 19200 HMI Address 5 <---------> PLC 3 Firmware OS Image [V13.00.01.09] Setting inside the SIMATIC HMI KTP700 Basic DP panel ADDRESS: 5. Protocol: MPI There is: PROFIBUS, STANDART, UNIVERSAL BAUD RATE: 19200 Load project in the panel. No errors, request (Overwrite All) agree (check a box). Panel loaded, but there is no connection. All field input fields ####. [see Panel view ] Included and turned on-off terminators (6ES7 972-0BB42-0XA0). No links. I tried [port 0] & [Port 1] & No connections with panel. |
Last edited by: AutoGen_1001023 at: 02/10/2022 14:09:32 |
|
2/10/2022 4:48 PM | |
Joined: 4/15/2015 Last visit: 6/14/2022 Posts: 12 Rating:
|
S7-224Xp setting port [System Block] KTP 700DP basic setting [Connections] An experiment with the launch of the project from TIA Portal Simulation RT was also conducted. Using USB PPI Apparter.Communication is available.Holds to think that there is no PPI connection type in the KTP700DP panel menu, only MPI & Profibus. AttachmentFiles.zip (676 Downloads) |
Last edited by: Jen_Moderator at: 02/11/2022 09:16:12Removed links and added files as an attachment. Last edited by: AutoGen_1001023 at: 02/11/2022 12:45:14 |
|
Follow us on