2/10/2022 10:59 AM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi Brian W, Regarding the name of the WinCC server PC, I would not recommend you to change it after the installation of WinCC Professional, as it can cause numerous access errors to the SQL database (which has the name of the current PC). To download RT Professional, please see this link: RT Professional - Loading projects Hope this helps. |
A rating will be well appreciated. |
|
2/15/2022 10:29 AM | |
Joined: 8/3/2009 Last visit: 9/8/2025 Posts: 16356 Rating:
|
Hello BrianW If you do not use any coplex SIMATIC Net components like SoftPLC or SIMATIC Net OP cServer on the same system as the WInCC Prof RT. you do not need to download the Hardware in the PC Station. For WInCC Prof RT only you can just use a simple WinCC download: https://support.industry.siemens.com/cs/ww/en/view/88780011 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on