(0)| 2/21/2022 4:25 PM | |
|
Posts: 3 Rating:
|
Can you guys (Siemens Enployees) please explain how the "Trigger tag" function works. I want to start logging when a bit is true or flip-flopped from the PLC and need to start the logging this way. I must say, the configuration method in KPT screens is very weird compared to SCADA systems i usually use.
------------------------------------------------------------------------------------------ |
Last edited by: Eydun at: 02/21/2022 16:26:19Last edited by: Jen_Moderator at: 02/22/2022 08:58:25New subject after splitting |
|
| 2/24/2022 3:52 PM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello Eydun A Trigger Tag works with the Events of the tag that you can set in the global HMI tags section. there is an easy example with the goal to change a screen in Runtime. there you can see how it generaly works: LINK The most important is to use the aquisition mode -> Cyclic continous Then you can use the most systemfunctinos that are available or start also Script s as the Panel supports it. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on