2/28/2022 4:31 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, Download scope You can either download the entire project or perform a download for a specific device. • Downloading a project to the target system (all target devices) (Page 557) • Downloading CPU/drive unit to target device (Page 560) • Downloading a program subset and single units (sources) to the target device (Page 562) https://support.industry.siemens.com/cs/ww/en/view/109801494 Safe the existing project after upload. Then you have a backup strategy.. Without "RAM2ROM" machine starts without changes, after "PowerOff". |
With best regards, |
|
Follow us on