3/18/2022 11:18 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Jackcaress, You should have post this query in SINUMERIK CNC automation systems product conference since is is 840D SL NCU 730.3PN with integrated S7-300 PLC CPU 317F-3 PN/DP. From the attached snap, PP72/48 module is interfaced on ethernet bus. Sinamics drives are connected to 840D SL integrated CU unit via internal Profibus. The details can not be provided since image is not clear. Hope this helps. If you need more details, please revert. |
3/18/2022 12:53 PM | |
Joined: 3/12/2015 Last visit: 10/14/2024 Posts: 534 Rating: (15) |
If the problem is that the photo is not clear I can send a new one of wherever I have to, the thing is I'm not sure where the reference is from the drive modules |
Follow us on