3/20/2022 1:58 PM | |
Joined: 10/4/2017 Last visit: 4/21/2024 Posts: 40 Rating:
|
This may be my 5th topic I post on this machine in hand. Currently the hard drive is partitioned to C, D, E, and F. sorry for the long post. Regards, Attachmentvid_20220317_093355 (1).avi (328 Downloads) |
3/22/2022 10:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello mattar1989, According to information I do have, in PCU50 HDD operation depends on the motherboard & BIOS system of it. So when GHOST backup is taken all hardware as well as software data image is recorded. When user restore this image information on another HDD & tries to connect it with PCU50, during boot up sequence, it checks & tries to detect same hardware & confirm software compatibility. Now since your new HDD capacity is 160 GB, not sure if hardware & software supports it or not? Moreover, when GHOST is restored on new HDD, have you check partition capacity of new & original HDD? Did you receive any error when tried to restore GHOST? What I can suggest you is, try to get spare HDD with 40 GB or less than 40GB size, try to restore GHOST image (please observe, no any error should be displayed during restore data) & check. All the best. |
This contribution was helpful to
1 thankful Users |
3/29/2022 5:00 PM | |
Joined: 10/4/2017 Last visit: 4/21/2024 Posts: 40 Rating:
|
I managed to get the Hard Disk Drive with 80 GB (exact same capacity of the original).
|
This contribution was helpful to
1 thankful Users |
Follow us on