3/28/2022 1:04 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating: (0) |
Hello Please what is the probleme in this script ?? |
Last edited by: ESCANOOR at: 03/28/2022 17:12:58 |
|
3/29/2022 10:20 AM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Hi ESCANOOR, |
3/29/2022 12:37 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating: (0) |
hi mirip sorry i tryed but it's not the solution of the probleme .. it's stiil the same message in the error window |
3/29/2022 2:25 PM | |
Joined: 9/3/2008 Last visit: 5/15/2024 Posts: 921 Rating: (158) |
Hi ESCANOOR The correct spelling is "ADODB.Connection" Also, remove the line: Set rst=connextion I hope this helps ;-) Regards |
Michael |
|
3/29/2022 5:27 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating: (0) |
hi michel sorry it's not usefull .. itryed but it still the same errors thank you |
3/30/2022 1:22 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello ESCANOOR please have a look at the official application example: https://support.industry.siemens.com/cs/ww/en/view/26283062 Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/30/2022 1:46 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating: (0) |
hello Murof thank you for the link is full of information but it still the same .. i don't know what's syntax error is best regard |
4/6/2022 1:50 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello Of course it is full of information because this is what you need. You cannot create a customized solution without knowing whats going on. The example in the Link is an officialy tested and working script example. you can easily compare. You can also use an internal Tag which you set to a specific value after every relevant script line. then you know exactly where the error is if you do not want to work with OnError...resume...next... Bye Murof |
Last edited by: Murof at: 04/06/2022 13:51:16If this Information really helps, you could use the Rate function |
|
Follow us on