4/29/2022 10:31 PM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating: (13) |
Dear All, I´ve the same problem after try to download to my OS Server. This project was a migration from 8.0 version to 9.1 version. When my migration finished, I configured my redundant server and operator station, and then I downloaded to each device, then I add a redundant server and a Operator station to the multiproject. After that I compile and download to my main server and all was Ok. When in WinCC I change the name of my Clients because the name change, and add my other client in computer and then compile all was good, but when I try to download, database context does not exist or is invalid message appear. What was the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2022 11:04:54New subject after splitting |
|
5/2/2022 11:07 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Error this computer is in the client list project. Please Open the project on the server first is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
Follow us on