5/10/2022 8:49 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, You will have to use RS232/PPI multimaster cable. Here is a link with more information: How can you transfer a WinCC flexible project serially to a panel? Best regards, Wizard |
1/12/2024 4:18 PM | |
Joined: 4/15/2022 Last visit: 4/11/2024 Posts: 2 Rating: (0) |
Hello! How did you resolve the problem? I checked the link: How can you transfer a WinCC flexible project serially to a panel? - ID: 23787153 - Industry Support Siemens But could´t get it right anyway.... Im using PPI 901-3CB30-0XA0, sice my computer does not have a serial-port im using it with a serial to usb adapter to connect to my PC usb port. Im i using the wrong PPI cable, E-stand: 03 ? Kbaud rate is set to 19.2, PG/PC is set to : S7 online(STEP7) --> PC adapter.PPI.1 i also tried: S7 online(STEP7) --> Serial cable.PPI.1. I have also configured the COM1 port in PC and setting this in PG/PC. MP 177 DP in Transfer mode, only one channel enabled " Serial: via PPI RS232/PPI Multi-Master Cable " Like you, i have also tried with MPI/DP to USB cable without success. Would be overjoyed of your response. |
Last edited by: Jen_Moderator at: 01/15/2024 09:39:37Link optimized. |
|
Follow us on