5/14/2022 4:07 AM | |
Joined: 12/28/2016 Last visit: 9/13/2024 Posts: 434 Rating: (45) |
You need to transfer the update fraimver file to a usb flash memory, then connect the flash memory to the USB port panel and turn on the panel How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?Attachmentusb_transfer_v1_0_e.pdf (422 Downloads) |
Last edited by: Jen_Moderator at: 05/16/2022 09:11:35Link optimized. Last edited by: Jen_Moderator at: 05/16/2022 14:10:11PDF file added as an attachment. https://pnap.ir |
|
5/16/2022 8:44 AM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168)
|
Hello, I'm afraid you will have to sent the panel in for repair. Best regards, Wizard |
Follow us on