5/13/2022 5:04 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4203)
|
In attachment the complete tag table. But that only bool tags. For analog values you must use variables of the VM area of the LOGO! Bool = Vx.Y AttachmentTags_LOGO!--TIA.zip (393 Downloads) |
This contribution was helpful to1 thankful Users |
5/18/2022 5:52 AM | |
Joined: 4/28/2015 Last visit: 8/29/2024 Posts: 3 Rating: (0) |
Thank you |
5/18/2022 6:03 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4203)
|
For more information to the VM area use the Online Help. |
5/18/2022 6:59 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33827 Rating: (4203)
|
In attachment a little example. LOGO!8.FS4 with KTP700 (TIA V13). AttachmentPI controller settings from HMI.zip (408 Downloads) |
Follow us on