4/10/2019 5:07 PM | |
Posts: 9 Rating: (1) |
Hi Denilson Where can I download the "Modbus TCP" Library for S71200 and TIA Portal v15?. Thanks Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/11/2019 6:16:42 AMNew subject after splitting |
|
4/11/2019 8:55 AM | |
Posts: 1283 Rating: (105) |
MB TCP application example thread the project shared there is been upgraded to v15 as attached. Read the thread and use the attached example project to try how it works.
AttachmentMODBUS TCP 1200 V4_V15.zip (1186 Downloads) |
4/12/2019 12:43 AM | |
Posts: 9 Rating: (1) |
Thanks Kirschiaub08 Actually I don´t have the Item "Modbus" in the "Comunication" folder. Best Regards tegra |
Last edited by: tegra at: 4/12/2019 12:47:12 AM |
|
4/12/2019 12:46 AM | |
Posts: 9 Rating: (1) |
Thanks Jay Can I copy and paste the MB_SERVER and the DBs of the example project? Because I don´t have the "Modbus TCP" library installed. Best Regards tegra |
5/20/2022 7:23 PM | |
Joined: 1/11/2022 Last visit: 6/23/2022 Posts: 2 Rating: (0) |
Oh! Ok Noddles, thanks for your advice. Regards, Martin |
Follow us on