5/21/2022 10:20 AM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33838 Rating: (4205)
|
Try this. Read the help to the blocks and try to understand. AttachmentWatchdog_0BA8.Standard.zip (480 Downloads) |
Last edited by: ixo65 at: 05/21/2022 10:21:12Attachment |
|
This contribution was helpful to1 thankful Users |
5/22/2022 12:46 PM | |
Joined: 1/6/2018 Last visit: 9/24/2024 Posts: 52 Rating: (1) |
Gentlemen ahnd ladies, I found this. I'm halfway there. Is it possible to keep the value stable, of the "data storage after 5 seconds" Counter, through the reset? Can I make a digital value, analog? If possible then I will just add an average and the thing is finished. AttachmentCircuit Diagram24.zip (431 Downloads) |
7/10/2022 7:59 AM | |
Joined: 1/6/2018 Last visit: 9/24/2024 Posts: 52 Rating: (1) |
Thank you Ilmarix This is how you store 2 temperatures and you extract their substraction in the way that if possitive = X1 and if negative = X2. In this example General sample time is 11s General Interlude time is 10s 1st sample time is at 5,01sec 2nd sample time is at 10,01sec Attachmentdifference temperature.zip (444 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on