5/18/2022 4:16 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
maybe wrong scout version with which sw the project was created? |
5/18/2022 4:26 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
maybe. scout V5.3.1.4 is on both system also the same Step7 version? |
5/18/2022 4:58 PM | |
Joined: 10/22/2011 Last visit: 4/3/2024 Posts: 297 Rating: (1) |
in my PC,Step7 is 5.7 in other PC, Step7 is 5.6 |
5/18/2022 5:16 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
afaik scout V5.3.1.4 was not released for Step7 V5.7. For this step7 version you must use Scout V5.4 |
5/18/2022 6:17 PM | |
Joined: 10/22/2011 Last visit: 4/3/2024 Posts: 297 Rating: (1) |
OK thanks I will inform you soon |
5/22/2022 6:56 PM | |
Joined: 10/22/2011 Last visit: 4/3/2024 Posts: 297 Rating: (1) |
Hello CristophD I installed Scout 5.4 and problem solved Thanks for support |
Follow us on