5/23/2022 3:27 PM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150)
|
Hello Aliiisa, If you want to have ready for use CFC tenplates, parameter lists and a detailed describtion, you can download the documentation"Configuration of SINAMICS and MICROMASETR Drives with Drive ES in PCS 7" Configuration of SINAMICS and MICROMASTER Drives with Drive ES in PCS 7 |
This contribution was helpful to1 thankful Users |
5/24/2022 11:52 AM | |
Joined: 5/6/2020 Last visit: 8/13/2024 Posts: 32 Rating: (1) |
Thanks Techno_Taru We have already read the manual for integrating the Sinamics G180 into PCS7 using Profibus, from the link below and set the parameters of the drive according to the manual. https://support.industry.siemens.com/cs/pa/en/view/109474410 But the problem is the abnormal behavior while commanding via bus and we couldn't find anything about it in the documents. |
Last edited by: Jen_Moderator at: 05/24/2022 13:02:18Link optimized. |
|
5/24/2022 12:27 PM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150)
|
Hello, In which OB you have your drive program? |
5/26/2022 2:23 PM | |
Joined: 5/6/2020 Last visit: 8/13/2024 Posts: 32 Rating: (1) |
Hi OB35 and OB1 |
Follow us on