5/22/2022 5:35 AM | |
Joined: 8/19/2012 Last visit: 9/15/2024 Posts: 125 Rating: (0) |
Dear I have OP37 with protool software.as you knowthe OP37 Is obsolete now. so i want upgrade the software and the OP. SO please help me to do that.the source file available in the attachment best regard AttachmentPRO1.zip (455 Downloads) |
5/23/2022 5:33 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
op37 not supported. to which HMI Device you want to migrate |
5/27/2022 2:06 PM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728)
|
Hello ENG YCS so you have to go with the steps - Protool to WinCC flexible and Change the Device type - WinCC flexible to TIA Portal -> Change the devicetype Here are some information for migrating this two steps: https://support.industry.siemens.com/cs/ww/en/view/18796902 https://support.industry.siemens.com/cs/ww/en/view/49752044 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on