6/10/2022 9:18 AM | |
Joined: 6/19/2019 Last visit: 4/5/2024 Posts: 690 Rating: (72) |
Hello, First off all I think better use memory card if you need later do maintenance or upgrades and don't whant go to location directly. You can just send file to vendor and thats all. also read this topic with good solution TIP:S7-1500 Memory concepts Example: if PLC broken, vendor buy new one PLC insert old memory card and machine work again. If you whant to see how to transfer program to memory card watch video HERE |
6/10/2022 2:04 PM | |
Joined: 2/5/2015 Last visit: 9/27/2023 Posts: 127 Rating: (0) |
Hello, thanks for your answer... So, MMC is better specially for maintenance, ok! Like the video shows, we grag the project to the CARD, so program will be in the card. 1) Should we "record" the program also in the PLC memory or only in the CARD? 2) The PLC will "pull" the program from the card to run it? If you remove the card it stops or keep running? |
Follow us on