6/22/2022 5:47 PM | |
Joined: 6/22/2022 Last visit: 6/22/2022 Posts: 1 Rating: (0) |
Hi, Is there a preferred/recommended anti virus or malware protection solution for the M6 PG? Regards Joe |
6/22/2022 7:41 PM | |
Joined: 2/17/2020 Last visit: 9/19/2024 Posts: 1061 Rating: (192) |
Hi, To find out which security programs are released and tested with the software installed on your PG, you can use the Compability Tool and download the software version compatibility list, such as WinCC V7.5. The tested security programs can be found in the 'Virus scanners / Whitelisting row' of the list. Additional information that may be useful: Finally, I would take into account what is indicated in the following section of the Field PG M6 manual: SIMATIC Programming device SIMATIC Field PG M6 - Security information |
A rating will be well appreciated. |
|
Follow us on