5/27/2022 8:30 PM | |
Joined: 11/24/2018 Last visit: 5/6/2024 Posts: 28 Rating: (1) |
Hello experts! I have two used UPS1600 6EP4134-3AB00-2AY0. I would like to access the parameters via the web browser. I have enabled it in TIA Portal V16. I can reach the UPS' with TIA Portal and SINEC PNI. I can also ping them just fine. I can't manage to open the web browser in either Windows 10 or 7 environment, though. I have tried with different PG's and PC's too. The UPS' are working fine (I think) with their current setup, so I don't think they're faulty. I have read the manual and watched You Tube clips about it. I must be missing something. Please help! I have added a few screenshots to illustrate the problem. I hope this helps a bit. Many thanks, DBM Attachment220528 SITOPzip.zip (471 Downloads) |
Last edited by: DBME at: 05/27/2022 20:31:08Last edited by: DBME at: 05/28/2022 16:43:05Online with Shutdown service Last edited by: DBME at: 05/28/2022 16:44:11Last edited by: DBME at: 05/28/2022 16:49:56 |
|
5/28/2022 5:50 PM | |
Joined: 11/24/2018 Last visit: 5/6/2024 Posts: 28 Rating: (1) |
Hello experts! I have made a brief video clip to add to the posted pictures from earlier. I think it speaks for itself. Thank you! Attachment20220528_164959.zip (511 Downloads) |
Follow us on