6/30/2022 4:30 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32884 Rating: (4066)
|
The LOGO! 0BA7 use Ethernet TCP/IP with the S7 protocol. The S7 protocol was not made public by Siemens. |
6/30/2022 9:55 PM | |
Joined: 2/17/2022 Last visit: 7/5/2022 Posts: 6 Rating: (0) |
S7 protocol and S7 comm(iso/tcp) is the same thing? |
7/1/2022 10:35 AM | |
Joined: 2/17/2022 Last visit: 7/5/2022 Posts: 6 Rating: (0) |
I have Beijer x2 pro 10 inch. |
Follow us on