7/2/2022 4:10 PM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12410 Rating:
|
Hello Tanay; ProTool v6 was discontinued in 2010, so there are no software or licenses available on the market since then. - Product Discontinuation for SIMATIC ProTool/Lite, ProTool, ProTool/Pro and ProAgent (2010) https://support.industry.siemens.com/cs/ca/en/view/42628254 In the same document you can see that WinCC Flexible was made available as a replacement software. SP5 was made available sin 2018, and is still in use today.There is therefore no requirement for a ProTool v6 license to run a WinCC Flexible project. There are various tpe of licenses you can purchase, Powertags Upgrades, Runtime... Could you describe your project with more details, so we can understand your requirements? Hope this helps, Daniel Chartier |
7/2/2022 6:19 PM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12410 Rating:
|
Hello Tanay; Since you have not given us any indication about your project it is hard to give you a simple Yes/No answer to your last question about the Simatic Automation Tool. This document describes the type of project help the Simatic AutomationTool can provide in v.4.0, Basic and Advanced. You should determine if it is useful to you. Notice that for HMIs it does not seem to offer more than centralized upload/download features... https://support.industry.siemens.com/cs/sa/en/view/98161300 Hope this helps, Daniel Chartier |
Follow us on