6/30/2022 9:46 AM | |
Joined: 5/7/2019 Last visit: 1/5/2023 Posts: 37 Rating: (0) |
Hello, We have other projects in which we use the free telegram, and then add the encoders actual position (r842). But I am not able to select the free telegram in the HW Config of Step7. Mind you: I am talking about a project in Step7, NOT in TIA Portal. I can select the free telegram in Starter, but I am not able to transfer this configuration to the HW Config of Step7. With kind regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/30/2022 14:11:34New subject after splitting |
|
7/1/2022 3:29 PM | |
Joined: 5/7/2019 Last visit: 1/5/2023 Posts: 37 Rating: (0) |
PLC: CPU17-2-DP With kind regards, |
7/5/2022 6:10 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980) |
use standard telegram 3 or 4 if you need encodervalues |
This contribution was helpful to1 thankful Users |
Follow us on