7/5/2022 7:06 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, I think there is a easy reason why the SFC is not working. Did you try to operate the SFC on the OS? If s, have you done a OS compile? And afterwards a OS download to the server (non Single Station)? Do you use control strategies? If so, did you set PARAM to "1"? Please send us a screenshot from the SFC in the CFC chart in test mode. |
Last edited by: Oreca at: 07/05/2022 07:09:19If I could help you, you can use the RATE button. Thank you. |
|
Follow us on