7/6/2022 9:24 AM | |
Joined: 4/26/2021 Last visit: 10/20/2023 Posts: 26 Rating: (3) |
I have two 400h cpu(CPU 414-5 H PN/DP) with two cp card(CP 443-1). I connected with these cp cards ip with wincc 7.5 as redundent connection. I did this with dynamic wizards.I placed two cp cards ip in main and reverse connection in dynamic wizards. But my connection does not switch when one cpu is stop. What Can I do?? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/06/2022 10:09:07New subject after splitting SML |
|
7/6/2022 10:10 AM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 949 Rating: (13) |
Closed cause question posted twice. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on