7/11/2022 3:19 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, the 5A DMoMo is compatible. In principle, SINAMICS S120 booksize C/D type Motor Modules are not dependent on SINAMICS firmware or STARTER versions. The replacement part successors have exactly the same data (power stack code, p0201, see the List Manual) as the respective booksize modules available today. Therefore, these modules cannot be distinguished from the SINAMICS firmware or the engineering tools. https://support.industry.siemens.com/cs/de/en/view/109480497 The conductors are different. You need an adapter or you have to replace the old contactor. e.g. Motor plug connector with push-in connection 6SL3162-2MB00-0AC0
|
With best regards, |
|
Follow us on