7/14/2022 2:33 AM | |
Posts: 1 Rating: (0) |
HI ALL...I would like to ask some help from you guys..... My company have a old model TP270 6inch , it suddenly went to black screen and cannot turn on, So we have bought a new one , but we only have the old protools file(in pdb format) and cannot open by winccflex, anyone can help me to convert the file to some format which can open by winccflex? or any method can convert this file to psb so that I can restore it directly from Prosave? I only have one TP270 and dont have other using spare. THANKS A LOT!!! [snip] AttachmentDOC.zip (518 Downloads) |
Last edited by: The Helping Hand at: 07/14/2022 13:05:05Link removed and added file as an attachment. |
|
7/15/2022 4:23 PM | |
Joined: 4/8/2021 Last visit: 9/20/2024 Posts: 638 Rating: (105) |
Hi denhk3280, I have found this in SIOS. Seems that there could be a chance to obtain the project but seems as it is a billable service. https://support.industry.siemens.com/cs/ww/en/view/109765132 Hope it helps. Br, Cocolino |
Best regards, |
|
Follow us on