8/4/2022 3:03 AM | |
Joined: 7/8/2022 Last visit: 5/14/2024 Posts: 12 Rating: (0) |
what do these messages mean? and how to remove them? |
8/4/2022 7:55 AM | |
Joined: 1/21/2013 Last visit: 9/18/2024 Posts: 3114 Rating: (486) |
Hi rinat1985, when STARTER is installed including help, the easiest way for getting help on a message is a double click on the message. You will find the same information at the list manual. Cause: The forced checking procedure (test stop) for the safe motion monitoring functions is currently in progress. Remedy: Not necessary. The message is automatically withdrawn when the test stop has been completed. When using safety integrated, a test stop for the motion monitoring functions is required. The message is only shown, as long the test stop is running. Usually you can ignore this message. Kind regards |
8/4/2022 11:45 AM | |
Joined: 7/8/2022 Last visit: 5/14/2024 Posts: 12 Rating: (0) |
all messages cleared after manual start |
Follow us on