8/16/2022 4:49 AM | |
Joined: 8/3/2022 Last visit: 12/22/2022 Posts: 4 Rating: (1) |
Hi everyone, I'm new to Siemens and I'm trying to enable a G120VFD using SINA_SPEED on Tia Portal v17. The PLC I'm using is an S7-1200 PLC. I've wired an ON and OFF Push Button to the PLC and 3 x 24V Digital signals to the PLC inputs to control the VFD speed. Once online I've observed that the Speed SP gets set as per the combination of the 3 x Digital bits seen in the ladder logic attached. However an output on the SINA_SPEED block viz. "AXIS ENABLED" remains FALSE regardless of the state of the input "ENABLE AXIS". At the same time an output on the SINA_SPEED block "ERROR" goes High as well. I'm able to see the speed on the VFD screen but can't get the VFD to Run despite Enabling it. Can someone please suggest a way ahead. Thank You, Anthony AttachmentPLC_Prog.pdf (569 Downloads) |
Follow us on