8/15/2022 4:22 PM | |
Joined: 10/16/2020 Last visit: 5/31/2024 Posts: 122 Rating: (12) |
Hi, Make sure you comply with all the points indicated in the following FAQ. Especially how the communication buses are distributed. - Redundancy in WinCC V7.x and WinCC Professional https://support.industry.siemens.com/cs/ww/en/view/109772627 BR. Cookie_M0nster |
If this information has been helpful to you, please don't forget to rate it. |
|
8/26/2022 6:34 AM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1659)
|
Hello masteryoda173 be sure that you check and set up all points of this FAQ on each System: https://support.industry.siemens.com/cs/de/en/view/868014 and also check the Redundancy state tags -> Check if the redundancy is working properly on both sides and if the Master/Standby state is shown correctly. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on