(0)| 8/29/2022 7:25 AM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello Jodossantos2 Yes without additional Information its hard to say whats the problem. The first beginning would be to check your time synchronisation: https://support.industry.siemens.com/cs/ww/en/view/69864408 then which alarms do you use? (Descrete alarms or PLC alarms like Program_Alarm) descrete Alarms are using the timestamp from the hmi systemtime. PLC Alarms using the systemtime from PLC and here you have to check if your local time settings are correct it there is something wrong... Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on