8/31/2022 4:47 PM | |
Joined: 5/31/2022 Last visit: 1/18/2023 Posts: 1 Rating:
|
We are using S7-300, S7-400 and S7-1500 systems, Can TIA portal replace the usage of Step 7 on these platforms? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/19/2022 11:54:39New subject after splitting |
|
9/1/2022 5:05 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
Hi, as Daniel Chartier already stated, with Step 7 Professional (for TIA) allows you to program S7-300 S7-400, S7-1200 and S7-1500 PLCs, so this may be usable for replacement of classic STEP 7. But in addition to that: If you have "very old" CPU-300 or other old hardware in central rack, this hardware may not be supported by TIA anymore and can not be configured with TIA. This is also the reason why some old projects with unsupported hardware can not fully be migrated into TIA. So in this case, STEP 7 classic is still needed, please have this in mind. TIA Portal Readiness Check Toolregards sancruz |
Feedback appreciated, please rate |
|
Follow us on