9/2/2022 9:43 AM | |
Joined: 5/23/2022 Last visit: 9/5/2022 Posts: 2 Rating: (0) |
These are our Controller and the BitSwitch we have to use |
9/2/2022 10:28 AM | |
Joined: 6/19/2019 Last visit: 9/5/2024 Posts: 697 Rating: (73) |
Hello, If i good understand you need define each input to desired temperature, so i will do with MOVE function each input with constant your defined temperature. and later sum all 10 bits value to PID setpoint see like this attached PDF AttachmentBlock_35 (FC34).pdf (312 Downloads) |
Follow us on