(0)| 9/13/2022 10:50 AM | |
|
Joined: 3/2/2015 Last visit: 1/15/2026 Posts: 67 Rating:
|
Hi Everyone, We are building a SCADA system with architecture as attached. All network components already exist except for SCADA. Network is MPI with 187.5k data rate. WinCC Advanced (Windows 10 Pro 64-bit) is being used for SCADA, CP5622 card will be used for communication with PLC's. I would like clarification on below queries. 1) Is any other software/hardware component required for establishing communication with the 6 S7-300 PLC's? 2) I came across another application with a similar configuration, but they were using SIMATIC OPC installed on the same PC running a custom-built monitoring application. Should I also be using SIMATIC OPC? what purpose does it serve? I understand that if I have multiple applications requiring the data from PLC then it may be wise to use an OPC server. Would I need SIMATIC OPC? 3) The customer wants to make the segment A to B in the attached drawing redundant. From what I recall MPI doesn't support redundant network configuration, converting to fiber optic and installing OLMs may be required. Is there any other solution to achieve segment redundancy? AttachmentRMS.pdf (180 Downloads) |
| 9/15/2022 3:50 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject WinCC Advanced and Multiple S7-300 PLCs over MPI is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
Follow us on