9/12/2022 9:36 AM | |
Joined: 9/7/2022 Last visit: 11/28/2022 Posts: 17 Rating: (0) |
Dear community, I have a program connect to factory i/o simulation, using plc 1214 ac/dc/rly control from hmi ktp700 basic pn. The program is to filling the tank automatically, and I want to make the setpoint to fill the tank is 250 as a default value in HMI display when I run wincc. I have already retain the plc tags and write default value in DB, but why plc always write the value back to initial (0)? Here's the picture in docx, thank you! Regards, Farkim AttachmentShare.docx (82 Downloads) |
Follow us on