9/21/2022 5:14 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
check the diagnostic buffer for errors |
This contribution was helpful to
1 thankful Users |
9/21/2022 5:59 AM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating:
|
Hi xuanngoc1100, if you do not have an installed TIA Portal, which is usually needed to read out the diagnostics puffer, you can also use the SIMATIC Automation Tool. This tool can be used without license for reading the diagnostics data. Of course, you can also download a trial version of TIA Portal (e.g. TIA Portal V17 trial) which can be used for 21 days. Please note: Siemens has to ensure full compliance with national, international and supranational regulations regarding export control and customs (ECC). Therefore, you need an additional registration for downloading export restricted software. Since this may take several days, you'd better use the TIA Portal trial if not already registered. This software comes without export restriction. Kind regards |
This contribution was helpful to
1 thankful Users |
9/21/2022 7:43 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
then plug it in again go online and check the diagnostic buffer |
9/21/2022 7:44 AM | |
Joined: 3/9/2022 Last visit: 7/13/2024 Posts: 8 Rating:
|
when the led blinks i can't go online in the diagnostic of tia v17. so i can't find the error code in the diagnostic,sir |
Follow us on