9/22/2022 2:57 PM | |
Joined: 11/4/2011 Last visit: 9/19/2024 Posts: 232 Rating: (26) |
Hi there! What you have here is a TO alarm 103, see here: https://support.industry.siemens.com/cs/ww/en/view/109781853/136082365067 For one, the complete error message should provide closer information about the detailed cause, so try getting the complete message. Also as you can see this is a configuration error (number range within 100), and as the manual states it can only be acknowledged by doing a TO restart. To do this, call MC_Reset, set its input Restart to TRUE, then execute it. Regards, |
This contribution was helpful to1 thankful Users |
Follow us on