6/6/2022 9:56 AM | |
Joined: 3/2/2007 Last visit: 4/12/2024 Posts: 924 Rating: (5) |
Kindly, can we activate and use the SOS safety function in Sinamics by triggering digital inputs on the CU320-2 control unit ? or do we have to do some special settings ? 6SL3040-1MA01-0AA0, SINAMICS CONTROL UNIT CU320-2 PN WITHOUT COMPACT FLASH CARD 6SL3054-0FB01-1BA0-Z F02, SINAMICS S120 COMPACTFLASH CARD WITH FIRMWARE OPTION PERFORMANCE-EXTENSION INCLUDING CERTIFICATE OF LICENCE V5.1 F02: 2x Safety license Extended Functions 6ES7515-2TM01-0AB0, SIMATIC S7-1500T, CPU 1515T-2 PN, Central processing unit with work memory 750 KB for program and 3 MB for data, 1st interface: PROFINET IRT with 2-port switch, 2nd interface, Ethernet, 30 ns bit performance, SIMATIC Memory Card required 6ES7954-8LL03-0AA0, SIMATIC S7, MEMORY CARD FOR S7-1X00 CPU, 3,3 V FLASH, 256 MBYTE |
... thank you ... |
|
9/28/2022 6:51 AM | |
Joined: 3/2/2007 Last visit: 4/12/2024 Posts: 924 Rating: (5) |
any ideas ? |
... thank you ... |
|
12/14/2022 11:32 AM | |
Joined: 3/2/2007 Last visit: 4/12/2024 Posts: 924 Rating: (5) |
Kind reminder |
... thank you ... |
|
Follow us on