9/27/2022 2:49 PM | |
Joined: 8/14/2013 Last visit: 4/19/2024 Posts: 47 Rating: (0) |
Do you have example of node-red communication via TCP/IP communication with the OUC ? Best I could establish is:
TCON setup: I tried setting up RemoteAddress and Remote port but then nothing works. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2022 07:31:57New subject after splitting |
|
9/28/2022 9:48 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, I was not able to use your flow as well. But it is possible to e.g. use the TCP-In node and the TSEND_C on PLC side. I attached a zip folder with two screenshots. Does this help? Best regards! AttachmentOUC.zip (504 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
10/6/2022 5:40 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, what datatype do you want to send to the PLC? I also have problems with strings. INTs are displayed strangely in the PLC, Bools work. Not really sure what to change to get a right format or get it to work at all in the String case. Attached my flow, but don't think this helps, as I have the same behavior. Best regards! AttachmentFlow_TSEND_TRCV.txt (434 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/9/2022 10:00 AM | |
Joined: 8/14/2013 Last visit: 4/19/2024 Posts: 47 Rating: (0) |
Thanks, I will check. I know for sure that it is possible to receive strings. |
Follow us on