10/13/2022 5:52 PM | |
Joined: 7/19/2022 Last visit: 10/8/2024 Posts: 398 Rating: (63) |
Hi Tecla, Apart from the SD memory card, the firmware update on an S7-1200 CPU and an S7-1500 CPU can be performed from V3.0 onwards via its integrated web server. I leave you a FAQ where it tells you how to do it: How do you perform a firmware update via the web server of the S7-1200/S7-1500? Here are also the latest firmware versions of the S7-1200 CPUs: Where can you find the firmware files for the S7-1200 CPUs? |
Last edited by: JBS98 at: 10/13/2022 17:57:41If this Information really helps, you could use the Rate function |
|
Follow us on