10/19/2022 10:36 AM | |
Joined: 8/12/2021 Last visit: 10/18/2024 Posts: 327 Rating: (30) |
Hi amartinez10! A slow response from a runtime can be due to several factors. Depending on what is causing the slowness, there can be several reasons. First of all you should make sure that the requirements are met (https://support.industry.siemens.com/cs/ww/en/view/109773506/128685289227). Do you have separate plant/system terminal and bus terminal? What is slow? Several possibilities: - Startup:https://support.industry.siemens.com/cs/ww/en/view/109485615 - Type of architecture? Single-user or client/server. In case of client/server: Do you have separate plant/system terminal and bus terminal? Plant: network through which you connect to the controllers. Bus: connection to clients/server. They must be on separate networks or it causes slowness (Invalid configuration). - Update of variable values (refresh) -> Look more at communication level: How it communicates, type of PLC, how many PLCs it connects with. - Loading an image: Slow to display image elements -> Do you use script? May affect the loading time of the images, does it happen in all images, in the images where it happens, are there many objects, are they dynamised, if there are many objects, does it affect the loading time? If there are many objects it affects. Does it take time to change from one image to another-> Does it use script? It may affect the loading time of the images. |
Last edited by: Jen_Moderator at: 10/20/2022 04:42:17Text formatting optimized. If this Information really helps, you could use the Rate function |
|
10/21/2022 12:53 PM | |
Joined: 10/19/2022 Last visit: 11/24/2022 Posts: 5 Rating: (0) |
Hello Murof and Swarley92, thank you for your answers.
In all screens. I attach the info of the main screen.
It's not slow here
Architecture Single-user server and separate server to use webnavigator (terminal server). In both servers is very slow (wincc runtime, and webnavigator client)
One S7-400, TCP/IP
Info attach.
We use scripts to change images, but we use buttons to activate/deactivate a binary variable without scripts, and it's slow. Greetings |
10/26/2022 12:22 PM | |
Joined: 10/19/2022 Last visit: 11/24/2022 Posts: 5 Rating: (0) |
up |
Follow us on