(0)| 11/25/2022 7:40 AM | |
|
Posts: 11 Rating:
|
Wincc and automatic export |
| 11/25/2022 9:26 AM | |
|
Joined: 1/21/2013 Last visit: 1/24/2026 Posts: 4432 Rating:
|
Hi Johnnyqn01, maybe these entry will help you: How do you export and import data in the XML format with WinCC (TIA Portal) Runtime Advanced? Kind regards |
| 11/25/2022 3:01 PM | |
|
Joined: 8/3/2009 Last visit: 1/23/2026 Posts: 16661 Rating:
|
Hello Johnnyqn01 you can use VB Script to write the data toa csv file: https://support.industry.siemens.com/cs/ww/en/view/106501825 Or you can try to use the MS automation interface like it is discribed int the WinCC V7 Manual (works also for Advanced RT (with a few changes)): https://support.industry.siemens.com/cs/ww/en/view/109792622/139193407371 (you have to install excel on the same system in 32 bit) or you work with OPC UA there are also examples for using Excel as OPC UA client Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on