12/12/2022 9:41 AM | |
Joined: 8/18/2020 Last visit: 4/9/2024 Posts: 14 Rating: (0) |
Hello - I need your help. I have IPC547G Pcs7 workstations and harddisk on this PC stop working, Ok I have backup from this PC over siemens tool USB - Paragon Hard Disk 15 (Suite). But i have only System backup ( Boot, Local Disk, System and WinRe). Now I try get restore on new harddisk over Paragon hard disk manager 15 (full launcher). Restore was done and partitions was maded (1.boot,2.local disk,3.system, 4.WinRe) .. but when I try turn PC system get blue dead with error 0xc0000225 with= required file is missing or contains error = windows\system32\winload.efi My question is .. can i do a successful system restore on new hard drive with only system backup partitions (boot,localdisk,system,winre)??? or i need full backup with all partitions on hard drive? Or can you help me with restore ? Am i doing something wrong? Thank you for your answers.. btw hard drive is the same like old one. Attaching some pictures for better understanding. AttachmentPictures.zip (527 Downloads) |
Last edited by: Thomas070 at: 12/12/2022 15:02:49 |
|
Follow us on