12/28/2022 6:14 PM | |
Joined: 6/1/2020 Last visit: 5/13/2024 Posts: 37 Rating: (0) |
I am seeing this example: https://support.industry.siemens.com/cs/document/22701694/what-options-are-there-in-wincc-flexible-for-using-a-multi-panel-or-mobile-panel-as-an-opc-server-?dti=0&lc=en-WW It is a WinCC Flecible project with a MP370 panel that is configure to work as OPC server. It is what I want, because in my project I have the same. My idea it is first learn how to connect to the server, how the server is named, how to see the values of items and so. And then, develop a OPC client to read some items. For the tests, I am running the WinCC project in the runtime and the I run the OPC Scout and I see this: In the OPC.Siemens.XML I can see MP370B, that is the prefix of the server that I have configured in the OPC XML Manager. But I get an error in the OPC Scout: E_IOPCBrowse.Browse, could not connect to the server. How could I connect to the server of the example with OPC Scout? |
Last edited by: GTSAGarcia at: 12/28/2022 18:33:08Last edited by: GTSAGarcia at: 12/28/2022 18:33:17Last edited by: GTSAGarcia at: 12/28/2022 18:34:15 |
|
12/29/2022 7:10 AM | |
Joined: 6/19/2017 Last visit: 6/4/2024 Posts: 8132 Rating: (165) |
Closed cause question posted twice. The second thread with the subject How to configura the OPC server in a MP370 panel? is published within the conference SIMATIC WinCC flexible. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on