(0)| 1/12/2023 9:07 AM | |
|
Posts: 1 Rating:
|
When using the edge applications IE Databus and IE MQTT Connector simultaneously or individually in the IEM, the following error occurs. If I want to connect to a databus via the IEM, I get a permanent load signal. If I want to connect to a device via IE MQTT Connector, the interface for IE Databus appears. The configuration of the bridge configuration is not displayed. IEM version: Versioniem-os-1.5.1-4-amd64 IED version: Version ievd-1.10.0-6-a AttachmentError_IEM_Databus_Connector (1).pdf (1316 Downloads) |
Last edited by: AutoGen_6588844 at: 01/12/2023 09:14:24 |
|
Follow us on