1/19/2023 9:34 AM | |
Joined: 11/7/2013 Last visit: 6/11/2024 Posts: 32 Rating:
|
Hello. I thought, that there is no secrets about GET/PUT communication, but still i cannot get it working in my case :D I want to have s7 communication betwen S71200 and S7 300 CPU 315 2-DP with CP-343-1 processor working as PROFINET controller. Both PLCs are i diffrent projects, S71200 in TIA Portal v13 and S7300 in Step7 Manager (HW config in attachment). Firstly I tried to do it like it was descripted in instruction I found on forum in different topic (added in attachment). It is about making in TIA Portal project DUMMY S7300 PLC with exact the same HW config and connect them. TIA Portal automatically create S7 connection between them. Then I should use this connection in PUT config and thats it. But CPU 315 2-DP i have is old one and it is not supported in TIA Portal and it is not available in hardware catalog. Different solution i found on forum is descripted on youtube ->https://www.youtube.com/watch?v=rMymTGXQClg&t=5s. It is about making S7 connection manualy. In attachment I added configuration I make in relation to youtube video. It is not working, in online diagnostic i see, that connection is offline. Do You have some ideas? What am I doing wrong? AttachmentMyPUTconfig.zip (156 Downloads) |
Last edited by: Jen_Moderator at: 01/19/2023 13:06:45Video embedded. |
|
Follow us on