2/1/2023 10:16 AM | |
Joined: 3/11/2019 Last visit: 6/14/2024 Posts: 1476 Rating: (266)
|
Hi, in your screenshot, only the "CONNECT" parameters are shown. These are used for connection handling itself, but this does not read/write anything. You have to use correct value for parameter "MB_MODE" to select which modbus function (read, write) should be processed. With the other block parameters you can decide which addresses should be read/written. But "where" (address/register) the values for "voltage, energy, ...)" are provided by the modbus server, should be described in it's manual. Description of MB_CLIENTMB_MODE, MB_DATA_ADDR and MB_DATA_LEN parametersregards sancruz |
Feedback appreciated, please rate |
|
Follow us on