2/23/2023 3:47 AM | |
Joined: 8/28/2021 Last visit: 5/11/2024 Posts: 30 Rating: (3) |
Hello AutoGen..., Note that the encoder connection diagram is not complete (See attached file). In this case the communication can be full duplex and the connection of the Master/Slave cables is crossover type (Tx-/Rx- and Tx+/Rx+). In addition, a key point is "For RS422, Pin 3 is RxD+ and Pin 8 is
RxD-" for the CM1241. Best Regards, AttachmentConnection to RS422 Master.pdf (517 Downloads) |
Follow us on