2/27/2023 8:20 AM | |
Joined: 7/9/2015 Last visit: 5/24/2024 Posts: 3848 Rating: (563)
|
Hi, We don't know what errors you are getting and if you are getting messages when you install the GSD, but I can give you some general information. The GSDML file structure is in compliance with the ISO 15745 "Open Systems Application Integration Framework" and must have a special structure. Perhaps your old files have some errors in this structure but new TIA Software carries out stricter control here - as example. GSD files should also always be certified. There are not so many informations about GSD Revisions but please check this FAQ for further informations: How do you install a GSD file and which GSD file version is released for which version of STEP 7 (TIA Portal)?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
2/27/2023 12:45 PM | |
Joined: 9/21/2021 Last visit: 5/14/2024 Posts: 6 Rating: (0) |
Hi, TIA Version 16.0, old gsd version1.18, ok gsd ver4sion 1.8. there are gsd files in attachment. AttachmentGSD.zip (157 Downloads) |
Follow us on