2/24/2023 10:50 AM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Dear Georg, It is nice to see you here. I have installed COMOS 10.4.3, which is the latest version, on Win2019 Server: I can confirm that it works fine, also the mentioned new driver has been installed by the main setup (setup.exe from the first directory of the full version of COMOS). In case it helps a bit, please have a look into the screenshots attached here. If you feel that the documentation should be checked/edited, please open a ticket at the COMOS support for that issue. All the best, SuperPippo Attachment24-2-2023.zip (526 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on